Good morning,
I have found some mistakes in the datasheet, version of april, for TPS92512.
page18. Value calculated for R1 is 175kohms datasheet recomends take the value 176 but in the equation 30 R1 value is 174kohms and the result 19.2 it's wrong. With a resistor of 176kohms R2 should be 20.74kohms.
page19. Equation 34 result is 89mA, but in the next equation it takes 88mA same in the equation 36.
I will be looking for more later :)
Regards