The design for an isolated driver using the LM3445 requires a discontinuous mode flyback transformer.
However, in treatments of this topology, there is usually a DC voltage specified that has a minimum and maximum value.
In designs and application notes for the LM3445, the schematic usually shows the rectified AC voltage feeding the primary directly without filtering bulk capacitors
So what is the assumed input voltage to the primary in this scenario, or minimum and maximum voltages?
In general, given the output power, how is the primary side inductance calculated?
At an LED power rating of 90 Watts, such that the LED voltage is ~38V @ 2.4 Amps would bulk storage capacitors be necessary?
Thanks in advance for any advice.
Wade