Hi ,
I will implement TPS61181 to drive 40 pieces of dual color (red and green)LED.
The maximum forward voltage of one piece LED is 3.7 volt.
There are two methods below,
1. 8 series using IFB1~IFB5. (20mA in each series and total are 8x5-=40 pieces).
2. 10 series using IFB1~IFB4 (20mA in each series and total are 10x4=40 pieces ).
I would like to know which method is better.
Thank you!