I am interested in LM3433 LED driver because of its common anode capability.
I want to drive maximum 28A on LED, so I thoroughly reviewed LM3433SQ-36AEV evaluation board. (up to 40A current drive)
But I found weird thing on the board layout. Q10~Q12 transistors (MMBT3904-7) seems to be flipped on bottom layer layout (fig. 8) MMBT3904-7 pin 1 is base and pin 2 is emitter, but I think that Q10 ~ Q12 on the layout are pin 1 emitter and pin 2 base.
So I think that this board works unexpected way about ENA node. If ENA pin is drove externally, it will work okay. But without external ENA signal, Q10~Q12 should make ENA signal when enough negative voltage is applied on -12V, but it will not work as expected, I think.
I don't have that evaluation board in my hand, so I just guess. Is there anyone who can check my finding is right or wrong??