Hello,
We would like to use the reference design PMP6024 (100-240VAC Input, 60W, 2-string, PWM Dimmable LED Driver) almost as it is. We are planning additional wireless connectivity but the 100-240VAC power supply part should be applied as it is.
There is a transformer used from Wuerth. As I can see it is custom one. Unfortunately the details are not described for it. Is there a change to get the data for it? The best way for us is when we could get the P/N for it and then we can order directly at Wuerth.
Description inside BOM for transformer looks something like that:
T1
450uH Xfmr, ETD Core, 450uH,64 Np, 26 Ns, 8 Na1, 10Na2,
ETD29/16/10 ETD29 14 Pin
Vertical
Wurth/Midcom
Thank you.
Best regards,
Vitezslav