We are using TPS92513 to drive 2 chains of 3 serial LEDs. We are able to dim the LEDs with PWM signal through PDIM pin. The frequency of PWM is 250Hz, with 256 steps from 0% to 100%. We are using IADJ to set driving current, the UVLO pin is open. The LEDs keep glowing when we decrease PWM duty cycle slowly to zero at 11-13V input voltage. We can totally turn off the LEDs when decrease duty cycle quickly at 11-13V input voltage or slowly at 15V input voltage. The LED glows when we power on the light at 11-13V input voltage with 0 duty cycle PWM. The LED turns off when we power on the light at 15V input voltage with 0 duty cycle PWM. We want the LED totally off when PWM duty cycle is 0.
There is a ~300mA spark at the rising edge of our PWM digital dimmed 230mA current. Is there any way to lower the current spark?
Thanks,
Bolin