Dear Sir
If I use LM3414 for 10% dimming ,the output current maybe under 350mA
so in this condition ,I can't use LM3414 for 10% dimming ,due to the output current will be under 350mA and over SPEC ,is it right ??
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
If I use LM3414 for 10% dimming ,the output current maybe under 350mA
so in this condition ,I can't use LM3414 for 10% dimming ,due to the output current will be under 350mA and over SPEC ,is it right ??
Thanks
I am not sure why they say 350mA in the datasheet. There is a graph of ILED vs RIADJ in the datasheet that shows you can set it as low at 100mA. We have done this and so have other people. You just need to make sure you are in CCM (inductor current never falls to zero) so it may require a higher inductor value. The equations are in the datasheet. You can also analog dim (also see datasheet) down to 100mA.
In either case you can dim much lower using PWM dimming. In fact you can go very low. For example, you choose RIADJ for 350mA output (or whatever you choose, but 350mA for this example) and the average LED current is approximately the duty cycle times the max LED current. So if you use a 10% duty cycle in this case the average LED current is 35mA.
The tolerance suffers a bit at lower currents because the error amp offsets become a higher percentage of the total current sense voltage. PWM dimming will not have that issue, the accuracy will not suffer. That is one reason it is often chosen for wide range dimming.