Hi,
I want to use a LP3944 with 8 LEDs. Some resistors are in series with the LED which set their current to 5 mA each.
However I see this in the datasheet :
The circuit is supplied with 3.3 V. My question is : can I supply my LED with 5 mA (which is less than 12 mA) with this device ?
If not, could you advise me another device that fits to my application ?
Thanks,
Guillaume