Dear all,
I'm using the LM3414HV for 24V 500mA LED drivers and I'm having some troubles when I connect multiple pieces of these drivers to a properly dimensioned 24V power supply.
The initial current absorption of these ICs sometimes lead the power supply to protection and then everything start to blink. In some configurations the blinking stops after few seconds, in some never stops. The only way to solve the problem is to change the power supply with one much more powerful than necessary.
The used schematic is almost identical to that indicated in the datasheet.
I'm thinking to modify the schematic by inserting some circuitry that pumps current in Radj at the start-up; the idea is to keep the output off until the initial transient is finished.
Does anyone has ever faced this issue or has some suggestion on how to solve it?
Thanks a lot!