Let's say I am using the CREE CXB1816 LEDs which require 35V @ 450mA:
Using the LM3466 this would allow me to create a Series string of two deep and then based on my constant current limits I could do several Parallels.
For illustration purposes using your example I will have two deep and five parallels, so this configuration will require 5 LM3466:
(Each 35V 450mA is equal to one LED)
35V 450m 35V 450m 35V 450m 35V 450m 35V 450m
35V 450m 35V 450m 35V 450m 35V 450m 35V 450m
So in this example I need a power supply that provides 2*35 = 70V and 5* 450mA = 2,250mA
Question: How do I determine the Cin, Cled, Rsen, Req,Ceq for my application.
I apologize if this is a BASIC knowledge question but I would appreciate any help you can offer.
Thank you, Denis