LM3409HV
Hello all,
I am designing a device using 4 LM3409, controlling a RGBW (Ledengin LZ400MD00) led.
Led current approx. 1A.
I want to use PWM dimming as well as analog dimming.
The latter is used for 2 reasons
- led-protection for the case its temperature is going out of control because the cooling medium (water) is gone. (yes I do measure the ledtemperature).
- To decrease the intensity of the led for the case the device runs in the dark and may blind the observer. (the device should work in daylight as well which needs much more light).
PWM dimming is done at a frequency of about 350 Khz ( 64 steps.).
(You may think that is ridiculous high, because our human eye is not able to see it, but believe me, in this application you can.)
That is why I have choosen to use parallel dimming.
When no light is to be emitted for a particular colour, EN pin will be pulled low.
For the time being I will only use one led, but in the future I would like to use a set of leds in series, and I am trying to make the same board suitable for that as well, possibly without changing components.
So the LM3409 could be used at Vin voltages from 12 to 50 V depending om the number of leds in series..
I use the schematics as in the datasheet, only the component values are adapted to my application.
Questions:
1) In the datasheet the Coff and Roff circuit is connected to V0. One of the reasons, I understand, is that the Vo varies with the current through the led, and will influence COFT.
Is there another reason?
However, when using multiple led’s in series, V0 changes and consequently Roff.
If Roff would be connected to another fixed voltage (e.g.11 V that is available on the board anyhow for other reasons), there is a real fixed Toff, that is not dependant on V0.
Is this true? What disadvantages are there
2) The circuit to prevent max Toff I don’t understand.
I assume Vo and VDD both >> 1.24 V.
If the DimFET shortens the LED, Vo = Lled*RDS(on). (say 0,3V). Diode is not conducting,
COFF would be charged by VDD and Toff depends on Roff2 only (fsw >>fdim).
If DimFET is open, Vo = Vled(fw). COFF would be charged partly by Vo, partly by VDD, dependent on the ratio of VDD and Vo. Hence TOFF depends on both Vo and VDD.
I cannot figure out how Roff2 is calculated, nor do I understand that any voltage for VDD > 2V is appropriate.
Do I miss something? Can anybody explain?
3) Indeed, when using parallel dimming requires measures during shorting the led.
What circuit could I use to get proper TOFF during close/open DimFET?
Or would my suggestion in 1) work?
Thanks in advance.
Led current approx. 1A.
I want to use PWM dimming as well as analog dimming.
- led-protection for the case its temperature is going out of control because the cooling medium (water) is gone. (yes I do measure the ledtemperature).
- To decrease the intensity of the led for the case the device runs in the dark and may blind the observer. (the device should work in daylight as well which needs much more light).
When no light is to be emitted for a particular colour, EN pin will be pulled low.
1) In the datasheet the Coff and Roff circuit is connected to V0. One of the reasons, I understand, is that the Vo varies with the current through the led, and will influence COFT.
Is there another reason?
However, when using multiple led’s in series, V0 changes and consequently Roff.
If Roff would be connected to another fixed voltage (e.g.11 V that is available on the board anyhow for other reasons), there is a real fixed Toff, that is not dependant on V0.
Is this true? What disadvantages are there?
2) The circuit to prevent max Toff I don’t understand.
I assume Vo and VDD both >> 1.24 V.
If the DimFET shortens the LED, Vo = Lled*RDS(on). (say 0,3V). Diode is not conducting,
COFF would be charged by VDD and Toff depends on Roff2 only (fsw >>fdim).
If DimFET is open, Vo = Vled(fw). COFF would be charged partly by Vo, partly by VDD, dependent on the ratio of VDD and Vo. Hence TOFF depends on both Vo and VDD.
I cannot figure out how Roff2 is calculated, not do I understand that any voltage for VDD > 2V is appropriate.
Do I miss something? Can anybody explain?
3) Indeed, when using parallel dimming requires measures during shorting the led.
What circuit could I use to get proper TOFF during close/open DimFET?
Or would my suggestion in 1) work?