When operating the TPS92512 with an LED lamp that requires output voltage somewhat near the input voltage (say only 2-5V below) performance becomes unstable when dimming from full brightness (it's fine at full brightness) via PDIM (a known phenomenon, see the spec section 8.4.3). It would appear that trade-offs for this include the inductor, the switching frequency, and perhaps the boot cap, is there some help/advice on selecting these parts, that is understanding the trade-offs? My system involves an input voltage range of 50-57 V and an unknown but wide output voltage range (perhaps 20 - 48V where the input has to be TBD V above the output).