Hello,
Is it possible for me to use the LM3406HV with a solenoid as the load instead of an LED?
The solenoid characteristics are below:
Inductance: 22mH
Resistance: 7.01Ohms
Thank you,
Jared
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I don't see why not, it is a current source. I am not sure how transient behavior would be with such an inductive load, but the LM3406 does have very fast response. There should be EVMs available to test with.