I am driving 1.08A total out using the TPS61196 with 4 LED string drivers driving one LED string. I have the drivers in parallel to get the total current needed for the string. The design seems to work fine except for when I increase the PWM duty cycle on the four string drivers (all connected to the same PWM) from <50% to full-on (100%) suddenly. As a result, the LED driver appears to begin indicating a fault every 184ms, followed by a retry to start the boost switcher up again, and then a repeat of the same scenario every 184ms. The fault/retry condition seems to point to a UVLO fault because it's not getting hot, and the ISET pin is not shorted to GND. The only fault/retry condition left is the UVLO. However, I have monitored Vin during this scenario and verified it never falls below 10.6V. The UVLO fault condition is 7VF max Vin falling, which appears to not be occurring. Thus, I cannot figure out why the chip is doing this.
Here are the relevant design specs:
Vin = 12V
Vout ~ 36V
Iout ~ 1.08A
Iset = 270mA, FBP = 4.8V, IFBV = 0.7V, Vovp=50V