Hi team,
I have a question for LP8860 VSYNC pin. In datasheet, we can know it is used with VSYNC and HSYNC signal. I am confused when to use HSYNC and VSYNC. And how to choose the bandwidth of loop filter and why.
Regards
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I have a question for LP8860 VSYNC pin. In datasheet, we can know it is used with VSYNC and HSYNC signal. I am confused when to use HSYNC and VSYNC. And how to choose the bandwidth of loop filter and why.
Regards
Michael
Hi,
VSYNC pin input works as a reference clock for internal PLL. Internal PLL can be driven from internal oscillator or external clock(VSYNC).
The reason there is VSYNC input is to synchronize internal timing with frame rate or line rate(HSYNC) of display to avoid waterfall effect which happens by interference between LED backlight and LCD display. In old days, LCD characteristics were not as good as current LCD, so the waterfall effect was bigger, but most of our LED driver have phase shift function which shift the phase of each LED string, so resulted LED freq becomes much higher. This improves waterfall effect as well as the improved LCD design itself.
Please refer to this picture how external timing signal is used.
And this is the table for filter component selection.
Filter components only needed when VSYNC input is used. Otherwise, it can be open.
Hope this helps,
Hi Michael,
Do you want to set I_LED with external resistor or use external temperature sensor for temperature degrading?
If it's for former, you can use this formula. 12 bit register setting for current, 3 bit scale, 4 bit correction factor can be ignored if you only use Riset for LED current setting. Just use 3000*Vbg/Riset
For example, if 24kohm is used, 3000*1.2/24 = 150mA
If you are talking about Iset at NTC description, it is pull down current to detect current setting, not I_LED itself, so the value is uA scale.
Hope this helps,
Yoon,
Thanks. I am talking about the Iset in NTC description. And I want to use RISET to limit the max current to 120mA now.
I am a little confused. I though the IC detect the NTC voltage and get temperature information. Then control the current and lower down the current to cool down the screen. So I don't know the relationship between Iled and Iset in NTC description. Because the Itemp is very small, just uA scale, it affects the Iled not very obviously...
like others said,
///////
Iset = 1uA,
Itemp ≈ 40uA.
and ILED = (1-40)uA + 150mA ≈150mA,
I don't know how to make connection between this calculated result to the knee point.
Even though the temp is 110deg, according to the formula,
Iset = 1uA,
Itemp ≈ 51uA,
and ILED = (1-51)uA + 150mA ≈150mA,
This is not as the current de-rating curve.
///////
Could you please kindly tell more detail about it?
Regards
Michael
Hi,
Iset = Vbg/(50*Riset)*1000 : Riset in kohm, Iset in uA
as shown in datasheet and max current will be
max current setting from current scale * LED_CURRENT_CTRL[11:0]/4095
If you don't have any preference of NTC function, I think PWM mode derating(shown as below) by NTC will be simpler and straightforward.
Current mode derating using external resistors and NTC is more complicated and derating characteristics are changing with NTC parameters which is hard to support various NTC options.