Dear Sir
May I know LM3549 support each channel 700mA or total 700mA ??
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kai
The LM3549 is a sequential driver so only one current sink can be enabled at a time which makes the total 700 mA.
Each driver can sink up to 700 mA with the typical on time being ~50% Green, 20% Blue and 30% Red.
Let me know if you need anything else.
Best regards,
Randy