Hi,
Iam using LM32674 EVM. I am seeing glitches in the LED current as well as inductor current. Please see waveforms below.
The setup is : VIN = 3.7V, 3P5S congif, duty cycle of PWM = 6%, rise/fall time = 5ns, Freq = 10kHz
The problem is threre for 6% duty . At higher duty, it vanishes and at lower duty it is lesser...most pronounced at 6%.
The current is 30mA maximum, so 6% = 1.8mA.