I am currently using the LM3414 to drive some LEDs. However, the need for the LM3414 to actually regulate the current has disappeared, and I will be controlling the LED current with a PWM signal from a microcontroller. However, there are still a lot of nice features in the LM3414 - a 65V MOSFET, gate driver, thermal shutdown, etc. I'm leaning towards continuing to use the LM3414, set the current to higher than I need, and drive the DIM pin with my PWM signal.
I'd basically be using the LM3414 as a combined MOSFET and gate driver, in one tiny package. I could use a separate gate driver and MOSFET but I have serious size constraints. Are you familiar with any devices that do this - combine a MOSFET and gate driver into one package, but without the extra circuitry of the current regulation?