Dear Sir
I will use OSRAM P2720 700mA LED (Vf=3V)
If we use 1pcs LED per channel (total 3 channel) and Vin range is 6V~36V
how to design this SPEC with SEPIC structure??
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The switch voltage would be 39V when the input voltage is 36V, but since it is a controller you can pick a FET with a higher voltage rating. It should be able to do 3V output with that input voltage range. You may want to use a lower switching frequency, maybe 250kHz to 350kHz, to make sure you have a low minimum duty cycle for 36V input.