Hi Team,
I need to drive the backlight LEDs for 3 different LCD screens. The three different screens have the following configurations:
My input voltage is 12V.
Ideally, I would like to have one SEPIC/Buck-Boost so I can use one setup to fit the needs of all 3 configurations separately (meaning I will never need to drive all 3 of these setups at one time, I just need one device that can be configure to the specifications of all 3 screens).
However, if there is not a SEPIC/Buck-boost that can fulfill this need, I am open to having one device that can accomodate for the boosting configurations (21V and 28V8) and another device that can meet the needs of the buck (9V).
Can you please recommend devices that will do the trick?
Thank you!!
Jared
Attached Datasheets for the screens: