Part Number: LM3433
Good afternoon.
I'm having a problem with the TI's driver LM3433 described on link below:
www.farnell.com/.../1640920.pdf
It was assembled with a 56 x 2.5 mm cable between driver and the led, and I'm using a 2kHz PWM pulse to control the led brightness with potentiometer setting to minimal current.
This system worked well for a while, but suddenly the driver smoked and stop working.
I think that the problem is the inductance of cable that probably is generating spikes and burning some components on the driver. The board has elements to add a snubber circuit to reduce this effects, but this elements are not specified on project file. So I would like to ask two questions:
1 - How could project the snubber circuit or find out the components values?
2 - How could I detect the burneds components on the board to replace them?
I apreciate your help.
Best Regards.
Bruno Borges