Hello,
I'm looking forward to the LED driver for meet the following specifications.
<Requirement 1>
Vin: 3.6V~6.8V
Vf=3.2V
LED=2S2P
ILED=1A
Analog Dimming
Can be used for 10ms~30ms Flash Operation
<Requirement 2>
Vin: 3.6V~6.8V
Vf=3.2V
LED=1S4P
ILED=1A
Analog Dimming
Can be used for 10ms~30ms Flash Operation
Can I use TPS92691 for the above specification if I seprate the conversion input voltage and the device input voltage?
I found that the LED driver which can be used for 3.6V of VIn(min), I would like to separate these voltages.
Please see the attached file.
TPS92691.pptx
Also, could you please let me know more suitable device for these requirement if there is?
Best Regards,
Ryuji Asaka