Other Parts Discussed in Thread: LM3410Hello TI-Community,
please can you give me some hints on a recommend boost or buck-boost chip for following requirements:
#1
Input: 1cell LiPo (3.0V - 4.2V)
Output 50..100mA (to be resistor adjustable during development) @ 1.5V - 8.5V (1 to 5 IR-LEDs)
if this is a to broad range of values
#2
Input: 1cell LiPo (3.0V - 4.2V)
Output 50..100mA (to be resistor adjustable during development) @ 6V - 8.5V ( == 4 to 5 IR-LEDs (Vf 1.5V-1.7V) )
and
#3
Input: 1cell LiPo (3.0V - 4.2V)
Output 50..100mA (to be resistor adjustable during development) @ 1.5V - 1.7V ( == 1 IR-LED (Vf 1.5V-1.7V) )
focus is on simple design (not on cost)
(and i will have to pair this with some LiPo charger and auto-power-off on battery empty...)
thanks for your support!
sunny greetings
stefan