Hello,
Are there the roadmap of LED driver for high current(Over 1A) strobe light?
This question is related to the following post.
https://e2e.ti.com/support/power_management/led_driver/f/192/t/575189
My customer is developing strobe flash.
The input voltage range of the battery (AA battery or lithium ion battery) is about 3.6 V to 6.8 V.
The output is 1A / Ch when flashing (10 to 30 ms lit) and 400 mA / ch at torch.
Now I am introducing TPS92691, I am using the PWM terminal for 1A / ch flash operation and I am considering making analog dimming at IADJ terminal during torch.
There are 1P4S, 2P2S, 4P1S etc. LED pattern.
Our customer request the roadmap of LED Driver for above requirement?
Best Regards,
Ryuji Asaka