Hello, I have a question about LM3466 and dimmable current sources. In the reference design, Rsen is selected in such a way that Vsen is kept around 0.3V. This is why Rsens=1 Ohm with 0.35A of driving current for each of the five strings is the evaluation board. Now my question is: if I use a dimmable current source with this evaluation board and I dim it at 10%, then I get 1/10th of the voltage across Rsens with respect of the initial configuration (0.035V, while the data sheet warmly suggests to keep Vsen around 0.3V). Does the module still work correctly even in this configuration? Are there any issues?
Thanks in advance.