Other Parts Discussed in Thread: TPS61197
Hi,
My customer has a question.
English data sheet P4 6.3 Recommended Operating Conditions,
"Analog and PWM dimming frequency 200 to 1000 Hz" is stated.
Does this frequency apply only to PWM dimming?
P16 Figure 9. Analog Dimming Linearity shows that,
There are descriptions "PWM Frequency 200 Hz, 5 kHz, 40 kHz"
P11 7.4.2 Analog Dimming Method shows that,
There are descriptions "For example, when the PWM frequency is 5 - kHz, C 5 equal to 1 - μF is sufficient."
From the above, I thought that there was no PWM frequency limit for analog dimming method.
Best Regards,
watanabe