Other Parts Discussed in Thread: LM5122,
I am using the above part in several applications, one of which the supply voltage for the LED string requires circa 60V+.
With my current choice of mosfets and switching frequency, the power dissipation in the device is too high and I have no margin for higher ambient temperatures that I require.
I know I can look at changing the mosfets and lowering the switching frequency but this is not ideal.
a) Can you feed VCC to the device from an external supply with a diode so the internal regulator is not used. I have used this technique with the LM5122 (page 15 of 5122 data) but not sure if this method can be used for the TPS part.
b) Could I feed Vin to the TPS form a lover voltage, say 12V but still have the have the LED string at 60V. From the chip block diagram this looks potentially possible.
Many thanks
James