This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP8860-Q1
Tool/software: Code Composer Studio
hello~
i have a question
I set EEPROM 0X86 to 0X6F
Vin = 12V, why Fault pin not high
i read 0x0F=0x40
In reply to matt chen:
In reply to Salome Ramirez Carrion:
Hello~I want to express , DISP_CL1_BRT and DISP_CL1_CURRENT two registers can be changedLED brightnessHow do I use these two registers to calculate current value and voltage value
Hi Matt,
DISP_CL1_CURRENT[11:0] sets the actual maximum current which can be same or lower than DRV_LED_CURRENT_SCALE[2:0] value, which sets the max scale or maximum current limit.
DISPL_CL1_BRT determines the brightness or duty % if BRIGHTNESS REGISTER is used as the display brightness mode, or it will also affect brightness % if PWM INPUT DUTY x BRIGHTNESS REGISTER mode is used.
Output voltage will be determine by your LED load forward voltage (typ 3V per LED) plus headroom voltage at the output pin ~1-2V.
Best,
Salome