I am having problems with the TPS92513 blowing up on power up at higher voltages. When applying power the TPS92513 fails and smokes. This happens when 36 volts is applied to the input of the circuit. This happens with both the HV and non HV parts. If voltage is slowly ramped up there are no problems. This problem happens on a hard power on. LED current is 300mA. To try fixing this I increased the inductance from 220uH to 470uH. The 470uH is an improvement, but it will still occasionally fails on a hard power on. Are there any suggestions on how to fix this so the TPS92513 does not fail on a hard power up?