I was running a thermal cycle test on my circuit. 300kHz switching and 1.5A drive current with 12VDC input and 3.1VDC output.
The thermal cycle test
Thermal Cycle Endurance Test:
- Input Voltage: 12VDC
- Low: -10°C
- High: 85°C@85%RH
- Ramp time: 1 minutes or at discretion of tester if test chamber cannot achieve 1 minute rise/fall time for temperature requirements.
- Dwell time: 10 minutes
After 72 hours the chip failed....kind of. The inner workings are a little mysterious, but i figure a diode check should give some useful information. Using a Fluke 85V i measured the diode with the black lead on Pin 6 and the red lead on Pin 7. on a working chip, I got 1.1V same when i put the red lead on pin 8, red lead on pin 9 i got 0.5V and a diode good beep.
On the bad chip I was reading 0.5V across all those points. Then i read short when i check the red lead to pin 7. Then, i read 1.1V and the chip worked again and i threw it back in oven.
Do you know what caused this to happen internally with the chip? is there some sort of re-settable fuse internally? or is this some weird anomaly that occurred?