Hi, team.
I have a question about TPS61196's specification value of electrical characteristic.
Could you tell me?
The recommended VOUT range of this device is VIN (MIN) to 120 V (MAX).
Is this 120 V decided by the boost ratio that comes from the minimum on time and the duty cycle?
<The question from the customer is this>
Although it is thought the rated voltage value of the IC is not related ( think from the peripheral circuit ),
How is the maximum value of the boost voltage decideed?
Best regards,
Masumi Sekiguchi