I am working on a prototype of a new design using the TPS92512. I was assuming the the ISENSE pin worked as a normal peak current comparator input and expected the voltage to reach a peak 0.300V and shut off the buck switch. What I see is the ISENSE voltage reaching approximately 0.430V. Looking a little closer at the datasheet, the ISENSE resistor setting should be 0.300V at the DC current you require, not the PEAK current.
Since the ISENSE pin is a sawtooth waveform, what part of the waveform is the IC is tracking? Is it 1/2 the peak-peak ISENSE voltage? Does Vin influence the set point? This is just a curiosity question more than a problem.