Other Parts Discussed in Thread: LM3409
Hi all
I have a design of a circuit with LM3409. It has one LM3409 and the rest of the design is the same as Manual recomendations.. The output of LM3409 is connected to 2 led string in pàrallel of 3 leds each.
My input and output I-V data are 12 V nominal input, 9 V nominal output, 2 A average led current per string, , 525000 Hz frecuency....
Also, I have an strobing pulse connected to EN pin. This pulse is 1000us long, and 25 Hz.
I have calculated the components values and the spice circuit is as follows:
My problem is that I have a delay in the rising up of the output pulse comparing with ENABLE pulse. You can see it in the graph below. The output pulse (yellow) does not follow EN pulse (pink). The output pulse rise up 300 us after the rise edge of EN pulse, and ends on time, so the output pulse long only 700 us aprox, not 1000 us as enable pulse. And I do not know why the rising edge has such delay.
Why such a delay is obtained in the output pulse? Any Idea
best regards