This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92638-Q1: Current setting and graph

Part Number: TPS92638-Q1

Hi,

In the TPS92638-Q1 datasheet, Iout is set by Vref/Rref *G.

When Rref=200Ohm, Iout is 1.222A.

But at figure 9. It is about 6mA.

Could you explain about this?

Thanks.