Other Parts Discussed in Thread: LM3492, TPS92560
Hello ,
I am designing a luminaire using LM3492 to drive four strings of duris S5 white LEDs ( LED VF is 6.1V and IF is 125mA). Currently i'm implement the configure 4S4P to LM3492AR111DEMO board and at 12VAC i can get the correct PF with 0.936 and the efficiency also nearest with 81%. By the way , i also have test with 24VAC , i can't get the good power factor. I would like to ask some question,please refer to below.
1) At 24VAC ,i need to change what component to make good power factor and efficiency.
2) At 32VAC ,i need to change what component to make good power factor and efficiency.
3) Is there have any solution or suitable application can drive up 12,24,32 VAC in good power factor and efficiency beside the LM3492.
Please help to advise.
Thanks.
Regards,
Loon