Other Parts Discussed in Thread: ASH
Tool/software: WEBENCH® Design Tools
Hi,
I used Webench to design an LEd driver for the following parameters:
Vin(min) = 9V DC
Vin(max) 30V DC
Iout- 85mA
Vout = 11.2 V ( 4 led in series CREE p/no: XQE series green)
Just cant get the circuit to work i.e will not regulate at the require current, or sometimes will work when voltage input is at 12V DC but will not regulate at other voltages. Need help please - first time poster - Would it help if I share the webench design ?
Thanks in advance:
Ash