I am currently working on a design using the TPS92691PWP part. The design is a fairly high power (cica 100W). (12/24v input). I am currently having an issue on power down with a very short current spike of around 3A on the LED chain (normally driven at ~2A)
What appears to be happening is that on power off, the input voltage drops rapidly, and hance input current (supplied bu the input caps) rises as the boost converter keeps trying to regulate the output. Due to this the inductor current limit is hit (~18Amps when using a 0.03 Ohm current sense resistor). This triggers a fault that turns off the output PWM FET. The Vout voltage seems to rise to 10V or so above the LED Vf (even though the switcher is off), and after ~35uS the fault is cleared so the output FET is re-enabled, dumping all the charge on the output caps through the LED chain - causing the spike.
Any ideas of how to stop this happening - other than implementing a higher UVLO on the PWM pin?