I have been working with the LM3409HV for some years now. I like it very much.
My parts have identical package code SYHB
Bath3 code: 73EJ
Bath1 and 2 code. 5C2V and 655F
When I test the behavior of my design I have been used to that the old batches (1 and 2) had a linear section (at the high currents values) that DID not pass through 0,0 of my plot, when the current was controlled at pin 2 Iadj.
My new batch (3) has now a linear section (at the high currents values) that DO pass through 0,0 of my plot, when the current is controlled at pin 2 Iadj.
All bathes still saturates at low Iadj values. Bath3 at a level > 0 Amps, Bath1 and 2 at a level = 0 Amps.
Can this be explained in any way
Best Regards
If schematics is required ask for them at fr@chemometec.com