Hi,
I don't understant why there are two different formula to calculate Iset current:
LP8861-Q1 datasheet : into 8.3.3.2 Equation 3 RISET= 2342 / (IOUT-2,5)
on Using the LP8861-Q1EVM Evaluation Module document paragraph 8.2 current setting is ILEd=2000X VBG /Riset for example on my application with 20mA for channel The Riset can be 120K or 134K. What is it the right formula? Do you have an excel file to calculate all value of LP8861 for my application ? 4 led driver @20mA for channel with Vin=24V. Thanks