Other Parts Discussed in Thread: LM3508, , TPS61158
Hi, team.
My customer using LM3508, now.
But , due to the following factors, the LM3508 is hard to use and needs to be replaced in the future.
Factor: The LM3508 will have some low current offsets due to the amplifier offset voltage impressed across the current setting resistor.
So only thing to ensure 0 mA current is to bring the enable input low.
(My customer want to be 0 mA current by DIM pin = L)
So question.
If TPS61169 is set to DIM pin = L, is ILED completely cut off?
Best regards,
Masumi Sekiguchi.