Tool/software: WEBENCH® Design Tools
I'm using a TPS92691 in a Buck-Boost application using the component values in Webench, and I'm finding the Gate Drive acting erratic.
The Gate output abruptly switches off (short duration) and then back on to complete the cycle (based on the Switching freq.).
The duration of the off time doesn't match the 35uS of the IS Fault, the IS line is staying under 525mV, and Soft Start is not indicating a Reset from a Fault.
The PWM pin is tied to Vcc and Iadj pin is tied to PWM through a 100K resistor.
The Vcc pin on the Driver has a very clean 7.5VDC.
Changing values of the Compensation components doesn't impact the timing of the problem.
What does help is increasing the output capacitance significantly beyond the Webench recommended value.
An additional odd thing to me in doing this, is that a Polymer Hybrid capacitor works better than multiple X5R ceramic capacitors in parallel.
I can't find anything in the datasheet that can explain why the driver would act this way.