Application:
Universal high power, high voltage Led-driver to be used in combination with several Ledstrips. Input voltage of the power rail: 65V. Maximum Ledstring-voltage: 40V, Maximum Led-current:2A. Maximum Ledpower:25W
Maximum ambient temperature: 80°C. The complete Led-driver is potted. Maximum measured temperature of the TPS92641: 115°C
Auxiliary 10V power rail available on the board. Switching Mosfets selected for low gate charge.
We want to reduce the temperature of the TPS92641 by reducing the internal power dissipation. As this is an existing design, we want to stay as close as posible to the original design.
Question: can we connect the auxiliary 10V (thru a diode) to the Vcc-pin? Any risk of damaging the controller (for instance because the Vin-pin drops to zero with the Vcc-pin still at 10V)?
Question: can we connect the auxiliary 10V to the Vin-pin with the top-Mosfet, Ron and RUDIM1 connected to 65V power rail? Looks (from the functional block diagram) like the Vin-pin is only used to power the internal LDO and the functional block generating some references.
Eric