Hi team,
I have a question about FB pin resistor.
The following description regarding FB pin is described
on page 5 of the datasheet.
"Boost/SEPIC feedback input; for normal operation this pin
must be connected to the middle of a resistor divider between
VOUT and ground using feedback resistor values from 5 kΩ to 150 kΩ."
Which resistor is a feedback resistor from 5 kΩ to 150 kΩ?
Is it a resistor between the FB pin and the mid point of R1/R2
when T shape (3 resistor) structure is needed?
Sincerely,
Tsuyoshi Tokumoto