Need a LED Driver (Boost: Vin-2.7-4.2V) that can push 8 LEDs ( in serial connection),
each LED have Vf (Voltage forward) = 3V max and If ( Current forward) =200mA.
It mean that for all LED (8 LEDs) the driver should be have 24V and 200mA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Need a LED Driver (Boost: Vin-2.7-4.2V) that can push 8 LEDs ( in serial connection),
each LED have Vf (Voltage forward) = 3V max and If ( Current forward) =200mA.
It mean that for all LED (8 LEDs) the driver should be have 24V and 200mA.
Hello Eli,
The only one I am aware of that could do this is the LM3410.
Regards,
Clint
Hello Eli,
Yes, that is the only device I am aware of that fits the specs you need. If the LEDs are 3V max it should be ok.
Regards,
Clint