Hi, team.
When TPS92641 is used by lower ripple current, it is unstable.
My condition is below.
Vin=72V
VIADJ=0.76V
Rcs=100m-Ohm
Rload=75-Ohm (Vout=57V)
L=1.5mH
When the inductor was changed to 330uH, it became stable. Why?
When a ripple voltage of a CS terminal is small, does it become unstable?
Best Regards,