Dear E2E member,
I want to find a Laser Driver solution.
Vin = 38V, VOUT = 80V, IOUT = 3A (constant current output)
Does TI have suitable solution?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Julian,
This will require a boost controller. We have 3 suitable devices: TPS92690, TPS92691, and TPS92692. Low side current sensing will be required so that the IC itself does not have 80V applied to it anywhere, but all 3 can handle these specs. They are all similar so which you choose would depend on what other features you may need.
Regards,
Clint
Hello Julian,
The CSP/CSN pins can common mode to ground so you can do low side current sensing. You can connect CSN to ground and CSP to LED- so it is at a low voltage and no pins on the IC will see the 80V output voltage.
Regards,
Clint