I'm trying to calculate the compensation components according to the equation in section "9.2.1.2.11 Loop Compensation" of the datasheet, but I get strange values.
I have 15 LEDs in the string. Current is 700mA. Voltage is 55V. My supply is 19V. Duty cycle = 67%. Dynamic LED impedance is 15ohms. L = 22uH. Cout = 10uF.
Using equations 39 - 44 on p25 of the datasheet, I get Rcomp = 671 micro-ohms, and Ccomp= 385uF!!
My fp is 1230Hz, and fzrhp is 61.9kHz. My Rsense is 0.2 ohms. My Risns is 0.022 ohms.
Can you tell me what I am doing wrong? I was expecting to get Rcomp ~= 500ohms.
By the way, the circuit works fine using the values in the datasheet: Rcomp = 510, Ccomp = 0.22uF.
I just want to understand why I get such strange values.
Thanks,
Richard