Hi Team,
I want to use boost to battery topology of TPS92602. My condition is as bellow, V battery is 24V , maximum LED Vf is 53V, minimum LED Vf is 21V and maximum LED if is 700mA. Is it suitable?
Janson
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I want to use boost to battery topology of TPS92602. My condition is as bellow, V battery is 24V , maximum LED Vf is 53V, minimum LED Vf is 21V and maximum LED if is 700mA. Is it suitable?
Janson
Hi Janson,
Yes, using SEPIC topology can meet that requirement. For SEPIC topology, the output voltage is the LED voltage.
Best Regards,
Shirley He