Other Parts Discussed in Thread: TPS92512EVM-001
Hi,
There is a diode D1 in the user guide of TPS92512EVM-001:
1. What is the diode use for?
2. What if remove this diode from circuit?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
There is a diode D1 in the user guide of TPS92512EVM-001:
1. What is the diode use for?
2. What if remove this diode from circuit?
Thank you.
Hello chentsu,
If the buck converter is running and you disconnect the LED string the buck inductor has current flowing. Where does that current flow? If there is an output capacitor it will dump its energy into the capacitor. If the capacitor is small or there is no capacitor the voltage will rise on the open end of the inductor until it finds a path to conduct. To figure out how high the voltage will go you use (1/2)L*I^2 compared to (1/2)C*V^2. The capacitor portion of the equation has to go from running V to final V so (1/2)L*i^2 = (1/2)C(V2^2-V1^2) where V1 is the operating output voltage and V2 is the final voltage after the inductor discharges.
With D1 in place the energy, once it reaches Vin plus a diode drop) will go to Vin preventing the open inductor from arcing, causing damage, or creating a safety concern.
Regards,