Hi
How to consider the rating of Rsense?
We suppose to be Vin=30V and ILED = 1.2A.
Could you please show us the way to estimate?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
That result will be larger than the actual power but can be used to size the resistor.
Power = Rsense * [Iled+(1/2)Ipeak2peak ]^2*maximumdutycycle. If the maximum duty cycle is 50% then the power rating will be half of the equation without the dutycycle in it.
Also, if the current ripple is a high percentage of the average current you would have to look up the equation for calculating RMS current in the resistor or use the RMS integral equation.
Regards,
Hello,
The calculation is correct but the resistor value is wrong. Please go through the datasheet on how to calculate the current sense resistor value. You will need to go through the design process because it will include the inductor value, switching frequency, Vin, Vled. You need to design the circuit to know what value the current sense resistor value will be.
Regards,